The Debug Sprite is invoked as follows:
> arm-none-eabi-sprite [options]device-urlboard-file
The device-url specifies the
debug device to use to communicate with the board. It follows the
standard format:
scheme:scheme-specific-part[?device-options]
Most device URL schemes also follow the regular format:
scheme:[//hostname:[port]]/path[?device-options]
The meanings of hostname,
port, path
and device-options parts depend on the
scheme and are described below. The
following schemes are supported in Sourcery CodeBench Lite for ARM EABI:
rdiUse an RDI debugging device. Refer to Section 6.5, “Remote Debug Interface Devices”.
flashproUse a FlashPro debugging device. Refer to Section 6.6, “Actel FlashPro Devices”.
alteraUse an Altera FPGA. Refer to Section 6.7, “Altera Devices”.
The optional
? portion is
allowed in all schemes. These allow additional device-specific
options of the form
device-options.
Multiple options are concatenated using
name=value&.
The board-file specifies an XML
file that describes how to initialize the target board, as well as
other properties of the board used by the debugger. If
board-file refers to a file (via a
relative or absolute pathname), it is read. Otherwise,
board-file can be a board name, and the
toolchain's board directory is searched for a matching file.
See Section 6.9, “Supported Board Files” for
the list of supported boards, or invoke the Sprite with the
-b option to list the available board files.
You can also write a custom board file; see
Section 6.10, “Board File Syntax” for more information about
the file format.
Both the device-url and
board-file command-line arguments are
required to correctly connect the Sprite to a target board.